Pure

Discretion meets a new dimension of hearing.

Whatever is going on around you, you shouldn’t have to miss out on a thing. So small that it is barely noticeable behind your ear, and available in a range of natural colors to match a variety of hair and skin tones, new Pure® hearing aids blend in perfectly.

Pure offers an outstanding binaural hearing experience, sophisticated features, and elegant design. The receiver sits directly in your ear canal and fits moderate to severe hearing loss, providing exceptional sound quality. Although Pure is small, it contains more features than any other hearing aid of its size — yet it has the industry’s lowest battery consumption*, so you can enjoy the best listening experience all the time without concerns about battery life.

A world’s first — enjoy better than normal hearing in demanding situations.

Pure is equipped with the latest version of BestSound™ Technology, an advancement considered a complete revolution in audiological engineering. Two independent clinical studies have stated you may even be able to hear better than people with normal hearing in certain difficult listening situations, like restaurants and cocktail parties.* Pure delivers a perfect balance of rich, natural sound quality and audibility. This technology is so advanced the hearing aids suppress wind noise, a common complaint among wearers.

To localize sound sources, maintain spatial orientation, and understand speech better, our brain utilizes information from both ears. This is especially helpful in noisy and challenging listening situations. Inspired by the advantages of hearing with two ears, or binaural hearing, Pure brings you cutting-edge technology to deliver the most natural listening experience possible.

Siemens Pure is packed with innovations:

  • Advanced Siemens BestSound™ Technology
  • Directional microphones that help you better focus on conversation
  • A superior binaural listening experience
  • Premium wireless connectivity for convenient control
  • Telecoil for connection and transmission of speech directly into your ears in facilities equipped with an induction loop, such as places of worship, theaters, or public buildings
  • A tinnitus therapy feature to help manage tinnitus and improve hearing at the same time
  • Convenient hearing aid with rechargeable batteries for hassle-free handling. Change batteries once a year instead of once a week
  • IP67-rated* for resistance to moisture, sweat, dust and dirt for greater reliability
  • Rocker switch for program or volume adjustments

Superb control and connectivity.

The touchControl App turns an Android™ or Apple® iOS® smartphone into a hearing aid remote control. Adjusting volume, treble and selecting programs is now possible with a free app. With a one-button press the easyTek™ streamer transmits audio from Bluetooth enabled and other audio sources into hearing aids.* The easyTek App turns a smartphone into a hearing aid control center; switching between TV and phone, or ‘zooming in” on a dinner companion while having dinner at a noisy restaurant has never been easier or more convenient.

Pure’s advanced technology delivers exceptional sound quality together with versatile features that help you enjoy the sound of life. Plus the rechargeable Pure hearing aid will make sure you’re always ready to go, whatever you’re planning.

*Two independent clinical studies have shown that Siemens hearing instruments with binaural processing provide better than normal hearing capabilities in certain demanding listening environments.

*For instruments with binaural processing.

*Achieved IP67 rating per IEC 60529 standard. Water-resistant device can be completely submerged in water up to 3 feet for 30 minutes and dust will not interfere with the satisfactory operation of the device.

“The Bluetooth® word mark and logos are owned by the Bluetooth SIG, Inc., and any use of such marks by Sivantos Group is under licenses. Other trademarks and trade names are those of their respective owners.”